Command/Query
:SYSTem:DATA:INSTruction:PICTure <String>
:SYSTem:DATA:INSTruction:PICTure?
This command sets the instruction picture shown to operator when TYPE = PICT.
|
Parameter |
String |
|
Description |
Instruction image |
|
Data Type |
Character string type (String) |
|
Range |
- |
|
Preset Value |
"" |
{String}<newline><^END>
Dim Var as String
Var = "D:\figure1.png"
Ena.WriteString ":SYST:DATA:INST:PICT " & Var, True
Ena.WriteString ":SYST:DATA:INST:PICT?", True
Var=Ena.ReadString
Edit Test > Edit Limit > Edit Measurement > Operator Instructions > Operator Instruction Setup > Picture > Select the picture image