Command Only
:SYSTem:TOPology:REFResh
This command can refresh the SPDT switch connection. Even if you connect SPDT switch after the test wizard is running, the SPDT switch may not be detected automatically.
This commands can detect the SPDT switch connections.
This function is added at the revision A.2.0x.
Ena.WriteString ":SYST:TOP:REFR", True
No Equivalent GUI