Other topics about Analyzing Data
The time domain function provides the following functions:
Transforming measurement data to data in the time domain (Transformation Function)
Deleting unnecessary measurement data in the time domain (Gating Function)
By using the Transformation Function, you can convert the results measured in the frequency domain to data in the time domain and analyze it.
To turn ON or OFF the transformation function, use the following command:
:CALC<ch>:TRAN:TIME:STAT
To select the transformation type (band pass/low pass), use the following command:
:CALC<ch>:TRAN:TIME
To select the stimulus type (impulse/step) when the transformation type is low pass, use the following command:
:CALC<ch>:TRAN:TIME:STIM
When the transformation type is low pass, you need to execute the following command because each measurement point must be a multiple of the start frequency.
:CALC<ch>:TRAN:TIME:LPFR
To set the window shape, use one of the following items.
|
Item |
Command |
|
β |
:CALC<ch>:TRAN:TIME:KBES |
|
Impulse width |
:CALC<ch>:TRAN:TIME:IMP :WIDT |
|
Rise time of step signal |
:CALC<ch>:TRAN:TIME:STEP :RTIM |
The above three items are dependent on each other. When the value of one of them is changed, the values of the other two are automatically changed to the corresponding values.
Unlike the manual operation, you cannot set the window shape by selecting the window type (maximum/normal/minimum). However, you can set the same shape as each window type by setting β as follows:
|
|
Maximum |
Normal |
Minimum |
|
Value of β |
13 |
6 |
0 |
To set the display range after time domain transformation, use the following commands:
|
Description |
Command |
|
Start value |
:CALC<ch>:TRAN:TIME:STAR |
|
Stop value |
:CALC<ch>:TRAN:TIME:STOP |
|
Center value |
:CALC<ch>:TRAN:TIME:CENT |
|
Span value |
:CALC<ch>:TRAN:TIME:SPAN |
You can use the Gating Function to delete unnecessary time domain data.
To turn ON or OFF the gating function, use the following command:
:CALC<ch>:FILT:TIME:STAT
To select the gate type, use the following command:
:CALC<ch>:FILT:TIME
To select the gate shape, use the following command:
:CALC<ch>:FILT:TIME:SHAP
To set the gate range, use the following commands:
|
Description |
Command |
|
Start value |
:CALC<ch>:FILT:TIME:STAR |
|
Stop value |
:CALC<ch>:FILT:TIME:STOP |
|
Center value |
:CALC<ch>:FILT:TIME:CENT |
|
Span value |
:CALC<ch>:FILT:TIME:SPAN |