Other topics about Communication with External Devices
The E5063A 24 Bit (Handler) I/O port provides the ports for data I/O shown below.
|
Port Name |
Usage |
Data Structure |
|
Port A |
Output |
|
|
Port B |
Output |
|
|
Port C |
Input/Output |
|
|
Port D |
Input/Output |
|
|
Port E |
Input/Output |
|
|
Port F |
Output |
|
Signal direction (input/output) can be changed for the ports C, D, and E as shown in I/O ports and control signal lines. Thus, before the ports are used, the directions should be determined according to their usage.
To specify the signal direction for the ports C and D, use the following command. Direction for the port E depends on the setting for the ports C and D.
|
Port Name |
Command |
|
Port C |
:CONT:HAND:C:MODE |
|
Port D |
:CONT:HAND:D:MODE |
When the ports C, D, or E are configured to input ports, binary data represented by High(0)/Low(1) of each bit of the port is read as decimal data.
To retrieve the data, use the following command as query:
|
Port Name |
Command |
|
Port C |
:CONT:HAND:C |
|
Port D |
:CONT:HAND:D |
|
Port E |
:CONT:HAND:E |
To ports A through F (the ports C, D, and E should be configured to output ports), binary data (decimal data when output data is specified with a command) represented by High(0)/Low(1) of each bit of the port can be output.
To output data, use the following command:
|
Port Name |
Command |
|
Port A |
:CONT:HAND:A |
|
Port B |
:CONT:HAND:B |
|
Port C |
:CONT:HAND:C |
|
Port D |
:CONT:HAND:D |
|
Port E |
:CONT:HAND:E |
|
Port F |
:CONT:HAND:F |
The bit 6 of the data output by :CONT:HAND:B (the bit 14 of the data output by :CONT:HAND:F) is ignored when outputting the /INDEX signal is turned ON.
The bit 7 of the data output by :CONT:HAND:B (the bit 15 of the data output by :CONT:HAND:F command) is ignored when outputting the /READY FOR TRIGGER signal is turned ON.