Show 

Timing Chart

Other topics about Communication with External Devices

Overview

This section shows the typical timing chart of I/O port Signal.

Timing chart of I/O Port Signal (Point Trigger: off)

 

Minimum value

Typical Value

Maximum value

T1

Pulse width of /EXTERNAL TRIGGER or External Trigger Input Port

1 μs

-

-

T2

Pulse width of /SWEEP END

10 μs

12 μs

-

T3

Time set as the trigger delay time

-

(See below note)

-

Timing Chart of I/O Port Signal (Point Trigger: on)

When the point trigger function is ON, the /EXTERNAL TRIGGER signal must be inputted for each measurement point during a single sweep. The /INDEX signal goes to the High level before starting measurement of the first measurement point and returns to the Low level after the completing measurement of all measurement points.

The /READY FOR TRIGGER signal goes to the Low level when the instrument is ready to accept the trigger signal for the first point and then goes to the High level when the trigger signal for the first point is received.

When measurement of all measurement points is completed and the instrument is ready to receive the trigger signal for the first point of the next sweep, this signal goes to the Low level again.

When the point trigger function is ON, the /READY FOR TRIGGER signal goes High each time a trigger signal is received and goes Low when measurement of each measurement point is completed and the instrument is ready to accept a trigger for the next measurement point.

The times of T1 and T2 are the same as those when the point trigger function is OFF. For more information, see Timing chart of I/O Port Signal (Point trigger function:OFF).

Timing Chart of Data Output and Write Strobe Signal

 

T1

Response time of write strobe signal

1 μs

T2

Pulse width of write strobe signal

1 μs

Timing Chart of Limit Test Result Output and Write Strobe Signal

 

T1

Response time of /PASS FAIL write strobe

1 μs

T2

Pulse width of /PASS FAIL write strobe

1 μs

Timing Chart of /INPUT1 and /OUTPUT1, /OUTPUT2

 

 

Minimum value

Maximum value

T1

Pulse width of /INPUT1

1 μs

-

T2

Response time of /OUTPUT1, /OUTPUT2

0.2 μs

0.4 μs