Other topics about Making Measurement
Use the :INIT<ch>:CONT command to turn ON the continuous initiation mode for the channels you want to measure and turn the mode OFF for any other channel.
Issue the :TRIG:SOUR command to set the trigger source to Internal trigger.
Use the :INIT<ch>:CONT command to turn ON the continuous initiation mode for the channels you want to measure and turn the mode OFF for any other channel.
Issue the :TRIG:SOUR command to set the trigger source to "Bus Trigger".
Trigger the instrument whenever you want to perform the measurement. An external controller can trigger the instrument by using one of the following three commands:
|
Command |
Can *OPC? command be used to wait for end of sweep? |
Applicable |
|
*TRG |
No |
Bus trigger only |
|
:TRIG |
External trigger |
|
|
:TRIG:SING |
Yes |
Repeat step 3 to start the next measurement cycle.