Source ON only during measurement (Initial Source Control Function)

The E5063A does not output the RF signal source while the measurement is hold. (when Initial Source Control is ON, default setting). This function allows you to output the signal source even while the measurement status is in hold.

    1. Press System > Service Menu > Init Src Ctrl to turn OFF.

Other topics about Setting Control Functions