Overload Detection and Power Trip Function

An overload detection and Power Trip function is a safety feature to protect your E5063A from over-input. The overload occurs when RF input is over 20 dBm. When an overload is detected, the measurement is aborted and the RF source signal is turned OFF, then the "Ovld Protection" is displayed on the instrument status bar.

Other topics about Setting Control Functions