Wait Time at Power Level Change

The E5063A have a wait time in measurement when the power level is changed in the following conditions.

This wait time function can be turned off.

The time can be adjusted. At default, it is 50 ms.

These setting are saved/recalled by state files.

Other topics about Setting Control Functions