Selecting Language

The drop-down button below Select Language label, provides you option between English, Traditional Chinese, Simplified Chinese, Korean or Japanese language. The language selection determines the language in which the Test Wizard will be displayed. However, the labels in the  measurement screen and the softkey menu displayed in the Advanced Mode are in default English language.  

This language selection is applied only to the Test Wizard area. The language for other area including soft keys, cannot be changed.

Other topics about Setting Up Test Sequence