Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).FILename = File
File = SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).FILename
This command specifies a file in which the information of network 1 to 4 (Nwk) (which you want to embed/de-embed using the 4 (or 6, 8)-port network embedding/de-embedding feature) is saved for the selected channel (Ch). The file is saved as a 4 (or 6, 8)-port touchstone file with the ".s4p" (or ".s6p", ".s8p") extension.
For information on network numbers, refer to Obtaining Characteristics After Embedding/De-embedding 4/6/8-port Network.
Specify the file name with the extension. When you use directory names (folder names) and file name, separate them with "\ " (back slash) or "/" (slash).
This function is available with the firmware revision 3.50 or above. The 6/8-port touchstone file is supported with the firmware revision 9.60 or above.
|
Parameter |
Nwk |
|
Description |
Number of network |
|
Data type |
Long integer type (Long) |
|
Range |
1 to 4
1, 2 (4-port touchstone file only) 3 (6-port touchstone file only) 4 (8-port touchstone file only) |
|
Preset value |
1 |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
|
Parameter |
File |
|
Description |
4/6/8-port touchstone file name |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Preset value |
"" |
|
Note |
When the processing type is set to NONE, even if the specified file does not exist, no error occurs when you execute this object. However, when you set the processing type to embedding/de-embedding with the SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk). TYPE object, an error occurs. |
Dim Emb As String
SCPI.CALCulate(1).FSIMulator.EMBed.NETWork(1).FILename = "network.s4p"
Emb = SCPI.CALCulate(1).FSIMulator.EMBed.NETWork(1).FILename
SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).TYPE
SCPI.CALCulate(Ch).FSIMulator.EMBed.STATe
Firmware 9.60 or above
Analysis > Fixture Simulator > De-Embedding SxP > Topology > User File (nwk1)|User File (nwk2)|User File (nwk3)|User File (nwk4)
Firmware 9.50 or below
Analysis > Fixture Simulator > De-Embedding S4P > Topology > User File (nwk1)|User File (nwk2)
:CALCulate{[1]-160}:FSIMulator:EMBed:NETWork{[1]-4}: FILename <string>
:CALCulate{[1]-160}:FSIMulator:EMBed:NETWork{[1]-4}: FILename?
{string}<newline><^END>
10 OUTPUT 717;":CALC1:FSIM:EMB:NETW1:FIL ""Network.s4p"""
20 OUTPUT 717;":CALC1:FSIM:EMB:NETW1:FIL?"
30 ENTER 717;A$