Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).TYPE = File
File = SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).TYPE
This command sets/gets the processing type for networks 1 and 4 (Nwk), for the 4/6/8-port network embedding/de-embedding feature for the selected channel (Ch).
This function is available with the firmware revision 3.50 or above. The 6/8-port touchstone file is supported with the firmware revision 9.60 or above.
|
Parameter |
Param |
|
Description |
Processing type |
|
Data type |
Character string type (String) |
|
Range |
Select from the following.
|
|
Preset value |
"NONE" |
|
Note |
Before selecting embedding/de-embedding, use the SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk). FILename object to specify the 4/6/8-port touchstone file in which the information on the network is saved. If you do not specify the appropriate file and you select embedding/de-embedding, a runtime error occurs and NONE is automatically selected. |
Dim EmbType As String
SCPI.CALCulate(1).FSIMulator.EMBed.NETWork(1).FILename = "network.s4p"
SCPI.CALCulate(1).FSIMulator.EMBed.NETWork(1).TYPE = "deem"
EmbType = SCPI.CALCulate(1).FSIMulator.EMBed.NETWork(1).TYPE
SCPI.CALCulate(Ch).FSIMulator.EMBed.NETWork(Nwk).FILename
SCPI.CALCulate(Ch).FSIMulator.EMBed.STATe
Firmware 9.60 or above
Analysis > Fixture Simulator > De-Embedding SxP > Topology > Type (nwk1)|Type (nwk2)|Type (nwk3)|Type (nwk4) > None|Embed|De-Embed
Firmware 9.50 or below
Analysis > Fixture Simulator > De-Embedding S4P > Topology > Type (nwk1)|Type (nwk2)> None|Embed|De-Embed
:CALCulate{[1]-160}:FSIMulator:EMBed:NETWork{[1]-4}:TYPE {NONE|EMBed|DEEMbed}
:CALCulate{[1]-160}:FSIMulator:EMBed:NETWork{[1]-4}:TYPE?
{NONE|EMB|DEEM}<newline><^END>
10 OUTPUT 717;":CALC1:FSIM:EMB:NETW1:TYPE DEEM"
20 OUTPUT 717;":CALC1:FSIM:EMB:NETW1:TYPE?"
30 ENTER 717;A$