Show 

Turning off ECal auto-detect function

The ECal module automatically detects the connection between E5071C's test ports and ECal module's ports. You can turn off this function to set ports manually.

  1. Press Channel Next/Channel Prev keys to select the channel for which you want to turn off the auto-detect function.

  2. Press Cal key.

  3. Click ECal > Orientation, and select Manual.

  4. Specify a test port of the E5071C.

  5. Specify an Ecal port for the port of the E5071C you specified.

  6. Even if the connection is wrong with the auto-detect function turned off, no error is displayed.

Other topics about Calibration with ECal