Holding Max/Min Points for the Trace

Maximum/Minimum trace hold function allows you to hold the active trace at the maximum or minimum point.

The procedure for setting the maximum/minimum trace hold function is as follows:

  1. Press Display > Data Hold > OFF|Minimum|Maximum

  2. Restart resets the trace.

Maximum/Minimum trace hold can be applied with several conditions:

Maximum/Minimum trace hold cannot be saved or recalled. Even when the maximum/minimum trace hold is turned ON and trace is saved, only the normal trace (Hold is OFF) is stored as trace data.