Saving the Screen Image to a File

Other topics about Data Output

Overview

Along with printing, the E5071C allows the user to save screen images as bitmap (.bmp) or portable network graphics (.png) files. Saved files can be loaded into PC application software for further processing.

Saving Screen Image as File

Follow the procedure below to save a screen image to a file.

  1. Display the screen to be saved as a file. If you want to save the screen with a white background, set the display mode to inverted display before saving the screen. For details about display mode, see Setting Display Colors.

  2. Press System key. The screen image at the time System key is pressed is the image that will be saved.

  3. Press Dump Screen Image to open the Save As dialog box. "Bitmap Files (*.bmp)" or "Portable Network Graphics (*.png)" can be selected as the file type.

  4. Select the file type.

  5. Select the destination folder and type a file name.

  6. Press Save to save the screen image of E5071C to a file.