Converting the Port Impedance of the Measurement Result

Other topics about Fixture Simulator

Overview

The measured value obtained by using a port impedance of 50 ohm can be converted into a measured value at an arbitrary port impedance.

Port impedance conversion function

 

Converting Port Impedance

  1. Press Analysis key, the click Fixture Simulator > Port Z Conversion.

  2. Specify the port reference impedance for the required port.

  3. Click Port Z Conversion to change the port impedance conversion function to the ON state.

  4. Click Return.

  5. If Fixture Simulator is OFF, click the key again to turn it ON.