An error message is displayed on a dialog box.
This message simply appears on the display, being not known to a remote environment such as a GPIB. This message is not displayed when another error (against a red background) has already been displayed in the instrument message/Warning area.
|
Messages |
Description |
|
TDR option is not found |
This message appears when the E5071C-TDR option is not installed completely or correctly. Reinstall the E5071C-TDR option. Restart the option. |
|
E5071C is not in TDR mode |
This message appears when E5071C-TDR option is not turned ON. Turn ON the E5071C-TDR option: Analysis > TDR - ON. If its already at ON state, then click Start TDR. |
|
Failed to connect <address> |
This message appears when there's start-up error in the E5071C-TDR option remote mode. <address> shows the specified VISA address. |
|
E5071C ENA option TDR already exist |
This message appears if E5071C-TDR option is turned ON when there's another E5071C-TDR option already turned ON and is running. |
|
E5071C is in SVC mode |
This message appears if E5071C-TDR option is turned ON when the E5071C is in SVC mode. |
|
Invalid state file |
This message appears when an invalid state file is recalled. Recall a valid state file, in *.tdr format. |
|
Latest E5071C firmware not found |
This message appears when E5071C-TDR option is run on older version of E5071C firmware. |
|
Unsupported revision |
This message appears when you recall the state file which is stored by newer revisions. The state file stored by newer revisions cannot be recalled. Update your TDR software with latest revision. |
|
Advanced/cal mode mismatch |
This message appears in E5071C-TDR option when you recall a setting which was saved in Advanced Mode, in Basic Mode. Note that, when you save the setting in the Advanced Mode, you cannot recall the file in the Basic mode. Recall the setting in the Advanced Mode. |