Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.STATe(Name) = Status
Status = SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.STATe(Name)
This command turns ON/OFF the balance-unbalance conversion function when the fixture simulator function is ON, for the selected trace of the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command. This function is available in the revision A.9.60 and above.
|
Parameter |
Name |
|
Description |
Trace Name |
|
Data type |
Character string type (String) |
|
Parameter |
Status |
|
Description |
ON/OFF of the balance-unbalance conversion function |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following.
|
|
Preset value |
False or OFF |
Dim BalMode As Boolean
SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"
SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.STATe("duptrace") = True
BalMode = SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.STATe("duptrace")
SCPI.CALCulate(Ch).FSIMulator.STATe
Analysis > Fixture Simulator > BalUn
:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:STATe <string>, {ON|OFF|1|0}
:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:STATe? <string>
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""
20 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:STAT ""DUPTRACE"",ON"
30 OUTPUT 717;":CALC1:FSIM:BAL:PAR1:STAT? ""DUPTRACE"""
40 ENTER 717;A