Property (Read-Write)
SCPI.CALCulate(Ch).PARameter.TNAMe.DEFine(Name) = Param
Param = SCPI.CALCulate(Ch).PARameter.TNAMe.DEFine(Name)
This command sets/gets the measurement parameter of the selected trace for the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command. This function is available in the revision A.9.60 and above.
|
Parameter |
Name |
|
Description |
Trace Name |
|
Data type |
Character string type (String) |
|
Parameter |
Param |
|
Description |
Measurement parameter |
|
Data type |
Character string type (String) |
|
Range |
Select either one of the following:
|
|
Preset value |
"S11" |
Dim MeasPara As String
SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"
SCPI.CALCulate(1).PARameter.TNAMe.DEFine("duptrace") = "S21"
MeasPara = SCPI.CALCulate(1).PARameter.TNAMe.DEFine("duptrace")
SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA
SCPI.CALCulate(Ch).PARameter.TNAME.SELect
SCPI.CALCulate(Ch).PARameter.TNAME.SPORt
Meas > S<XY> {X=1-4;Y=1-4}|
Meas > Absolute > R<X> {X=1-4}|A|B|C|D|
Meas > Aux Input 1|Aux Input 2
:CALCulate{[1]-160}:PARameter:TNAMe:DEFine <string>, {S11|S21|S31|S41|S12|S22|S32|S42|S13|S23|S33|S43|S14|S24|S34|S44|A|B|C|D|R
1|R2|R3|R4|Aux1|AUX2}
:CALCulate{[1]-160}:PARameter:TNAMe:DEFine? <string>
{S11|S21|S31|S41|S12|S22|S32|S42|S13|S23|S33|S43|S14|S24|S34|S44|A|B|C|D|R1|R2|R3|R4|AUX1|AUX2}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""
20 OUTPUT 717;":CALC1:PAR:TNAM:DEF ""DUPTRACE"", S21"
30 OUTPUT 717;":CALC1:PAR:TNAM:DEF? ""DUPTRACE"""
40 ENTER 717;A$