Method (Write-only)
SCPI.CALCulate(Ch).PARameter(Tr).SELect
This command sets/gets the selected trace (Tr) of selected channel (Ch) to the active trace.
You can set only a trace displayed to the active trace. If this object is used to set a trace not displayed to the active trace, an error occurs when executed and the object is ignored. (No read).
In revision A.9.60 and above, you can select the trace by the trace name, provided it has been defined earlier. To define a trace name, execute SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
In revision A.9.60 and above, you can execute the action directly by using direct channel and trace assign commands like SCPI.CALCulate(Ch).TRACe(Tr).XXXX.XXXX.
|
Parameter |
Tr |
|
Description |
Trace number |
|
Data type |
Long integer type (Long) |
|
Range |
1 to 16 |
|
Preset value |
1 |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
SCPI.CALCulate(2).PARameter(2).SELect
SCPI.CALCulate(Ch).SELected.CORRection.EDELay.MEDium
SCPI.CALCulate(Ch).SELected.CORRection.EDELay.TIME
SCPI.CALCulate(Ch).SELected.CORRection.EDELay.WGCutoff
SCPI.DISPlay.WINDow(Ch).ACTivate
SCPI.SENSe(Ch).CORRection.EXTension.AUTO.DCOFfset
Trace Prev / Trace Next
:CALCulate{[1]-160}:PARameter{[1]-16}:SELect
10 OUTPUT 717;":CALC1:PAR1:SEL"