Property (Read-Write)
SCPI.CALCulate(Ch).PARameter(Tr).SPORt = Value
Value = SCPI.CALCulate(Ch).PARameter(Tr).SPORt
This command sets/gets the output port used for absolute or AUX measurements, for the selected trace (Tr) of the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Setting of the output port |
|
Data type |
Long integer type (Long) |
|
Range |
1 to 4 |
|
Preset value |
1 |
|
Note |
You need to set the measurement parameter for absolute/AUX measurements with the “SCPI.CALCulate(Ch).PARameter(Tr).DEFine” command. |
Dim Sport As Long
SCPI.CALCulate(1).PARameter(1).DEFine = "B"
SCPI.CALCulate(1).PARameter(1).SPORt = 4
Sport = SCPI.CALCulate(1).PARameter(1).SPORt
SCPI.CALCulate(Ch).PARameter(Tr).DEFine
Meas > Absolute > A(x) ...D(x)...R1(x) ...R4(x) (x: 1 to 4)
Meas > AUX Input 1 or AUX Input 2 > Sweep Port
:CALCulate{[1]-160}:PARameter{[1]-16}:SPORt <numeric>
:CALCulate{[1]-160}:PARameter{[1]-16}:SPORt?
{value}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:DEF B"
20 OUTPUT 717;":CALC1:PAR1:SPOR 4"
30 OUTPUT 717;":CALC1:PAR1:SPOR?"
30 ENTER 717;A