Property (Read-Write)
SCPI.CONTrol.HANDler.OUTPut(Num) = Value
Value = SCPI.CONTrol.HANDler.OUTPut(Num)
This command sets/gets data to OUTPUT1 or OUTPUT2 of the handler I/O.
|
Parameter |
Num |
|
Description |
Number of the OUTPUT terminal |
|
Data type |
Long integer type (Long) |
|
Range |
1 or 2 |
|
Preset value |
1 |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
|
Parameter |
Value |
|
Description |
Polarity (High/Low) |
|
Data type |
Long integer type (Long) |
|
Range |
Select from the following:
|
Dim HdlPol As Long
SCPI.CONTrol.HANDler.OUTPut(1).DATA = 1
HdlPol = SCPI.CONTrol.HANDler.OUTPut(1).DATA
No equivalent key is available on the front panel.
:CONTrol:HANDler:OUTPut{[1]|2}[:DATA] {1|0}
:CONTrol:HANDler:OUTPut{[1]|2}[:DATA]?
{1|0}<newline><^END>
10 OUTPUT 717;":CONT:HAND:OUTP1 1"
20 OUTPUT 717;":CONT:HAND:OUTP1?"
30 ENTER 717;A