Property (Read-Write)
SCPI.HCOPy.SDUMp.DATA.FORMat = Value
Value = SCPI.HCOPy.SDUMp.DATA.FORMat
This command sets/gets the image format (print screen image).
This command is available at the revision A.11.0x and above.
This command appears on the VBA editor with Auto_complete_Feature, however, this is not supported on VBA/COM.
|
Parameter |
Value |
|
Description |
Image format |
|
Data Type |
Character string type (String) |
|
Range |
PNG|BMP |
|
Preset Value |
PNG |
|
Unit |
- |
|
Resolution |
- |
SCPI.HCOPy.SDUMp.DATA.IMMediate
No equivalent key is available on the front panel.
:HCOPy:SDUMp:DATA:FORMat {PNG|BMP}
:HCOPy:SDUMp:DATA:FORMat?
{PNG|BMP} <newline><^END>
10 OUTPUT 717;":HCOP:SDUM:DATA:FORM PNG"
20 OUTPUT 717;":HCOP:SDUM:DATA:FORM ?"
30 ENTER 717;A$