Parameter
Std
Description
Standard number
Data type
Long integer type (Long)
Range
1 to 21
Preset value
1
Note
If the specified variable is out of the allowable setup range, an error occurs when executed.