Property (Write Only)
SCPI.MMEMory.LOAD.CHANnel.STATe = Register
This command recalls the instrument state for an individual channel (saved with the SCPI.MMEMory.STORe.CHANnel.STATe object) from the specified register as the setting of the active channel.
|
Parameter |
Register |
|
Description |
Register |
|
Data type |
Character string type (String) |
|
Range |
Select from the following: "A": Specifies register A. "B": Specifies register B. "C" :Specifies register C. "D" :Specifies register D. |
|
Note |
If no instrument state has been saved in the specified register, an error occurs and the object is ignored. |
SCPI.MMEMory.LOAD.CHANnel.STATe = "a"
SCPI.MMEMory.STORe.CHANnel.STATe
SCPI.DISPlay.WINDow(Ch).ACTivate
Save/Recall > Recall Channel > A|B|C|D
:MMEMory:LOAD:CHANnel[:STATe] {A|B|C|D}
10 OUTPUT 717;":MMEM:LOAD:CHAN A"