Property (Write Only)
SCPI.MMEMory.STORe.SEGMent = File
This command saves the segment sweep table of the active channel into a file in the CSV format (extension ".csv").
Specify the file name with the extension. When you use directory names and file name, separate them with "\ " (back slash), or "/" (slash).
|
Parameter |
File |
|
Description |
File name to save segment sweep table (extension ".csv") |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Note |
If a file with the same name as the specified file name exists, its contents are overwritten. |
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.MMEMory.STORe.SEGMent = "d:\segm01.csv"
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.MMEMory.STORe.SEGMent = "test/segm01.csv"
SCPI.DISPlay.WINDow(Ch).ACTivate
Sweep Setup > Edit Segment Table > Export to CSV File
:MMEMory:STORe:SEGMent <string>
10 OUTPUT 717;":MMEM:STOR:SEGM ""Test1/Segm01.csv"""
10 OUTPUT 717;":MMEM:STOR:SEGM ""D:Segm01.csv"""