Property (Read-Write)
SCPI.SENSe(Ch).SEGMent.LIST.BWIDth.PORT(Pt).RESolution = Data
Data = SCPI.SENSe(Ch).SEGMent.LIST.BWIDth.PORT(Pt).RESolution
This command sets/gets the IFBW of each segment for the selected port (Pt) and channel (Ch). This command is supported in revision A.11.20 and above.
|
Parameter |
Data |
|
Description |
Sets/gets the port IFBW of each segment |
|
Data type |
Variant type (Variant) |
Dim SegmData As Variant
Dim IFVal1 As Variant
Dim IFVal2 As Variant
SCPI.SENSe(1).SEGMent.DATA = Array(5,0,0,0,0,0,2,100E6,2E9,31,2E9,3E9,100)
SCPI.SENSe(1).SEGMent.LIST.BWIDth.PORT.STATe = True
SCPI.SENSe(1).SEGMent.LIST.BWIDth.PORT(1).RESolution =Array(1E3, 7E3)
SCPI.SENSe(1).SEGMent.LIST.BWIDth.PORT(2).RESolution = Array(7E3, 1E4)
SegmData = SCPI.SENSe(1).SEGMent.DATA
IFVal1 = SCPI.SENSe(1).SEGMent.LIST.BWIDth.PORT(1).RESolution
IFVal2 = SCPI.SENSe(1).SEGMent.LIST.BWIDth.PORT(2).RESolution
SCPI.SENSe(Ch).SEGMent.LIST.BWIDth.PORT.STATe
Sweep Setup > Edit Segment Table > List Port IFBW
:SENSe{[1]-160}:SEGMent:LIST:BWIDth:PORT{[1]-4}[:RESolution] <value1>,<value2>,...,<value N>
:SENSe{[1]-160}:SEGMent:LIST:BWIDth:PORT{[1]-4}[:RESolution]?
{numeric 1},{numeric 2},...,{numeric N}<newline><^END>
10 DIM I(1:2,1:5)
20 DIM J(2)
30 DIM K(2)
40 OUTPUT 717;":SENS1:SEGM:DATA 5,0,0,0,0,0,2,1E6,2E9,31,2E9,3E9,100"
50 OUTPUT 717;":SENS1:SEGM:LIST:BWID:PORT:STAT ON"
60 OUTPUT 717;":SENS1:SEGM:LIST:BWID:PORT1 1e3, 7e3"
70 OUTPUT 717;":SENS1:SEGM:LIST:BWID:PORT2 7e3, 1e4"
80 OUTPUT 717;":SENS1:SEGM:DATA?"
90 ENTER 717;A,B,C,D,E,F,G,H,I(*)
100 OUTPUT 717;":SENS1:SEGM:LIST:BWID:PORT1?"
110 ENTER 717,J(*)
120 OUTPUT 717;":SENS1:SEGM:LIST:BWID:PORT2?"
130 ENTER 717;K(*)