Property (Read-Write)
This option is only available in revision A.9.60 and above:
SCPI.SENSe(Ch).SEGMent.LIST.CONTrol.DATA = Data
Data = SCPI.SENSe(Ch).SEGMent.LIST.CONTrol.DATA
This command sets/gets the state of each segment in the segment sweep table of selected channel (Ch).
This command is only available in revision A.9.60 and above.
|
Parameter |
Data |
|
Description |
Indicates the state array data; where N is the number of segments and n is an integer between 1 and N. Data = {<state1>,... ,<state n>,.... ,<state N>} |
|
Data type |
Variant type (Variant) |
Dim SegmContrData As Variant
SCPI.SENSe(1).SEGMent.LIST.CONTrol.DATA = Array(1, 1, 0, 0)
SegmContrData = SCPI.SENSe(1).SEGMent.LIST.CONTrol.DATA
SCPI.SENSe(1).SEGMent.LIST.CONTrol.DATA = SegmContrData
Sweep Setup > Edit Segment Table
:SENSe{[1]-160}:SEGMent:LIST:CONTrol:DATA <state 1>, <state n>, <state N>
:SENSe{[1]-160}:SEGMent:LIST:CONTrol:DATA?
Where N is the number of segments and n is an integer between 1 and N.
10 DIM H(1:3)
20 OUTPUT 717;":SENS1:SEGM:DATA 5,0,1,0,0,0,3,";
30 OUTPUT 717;"1E9,3E9,11,70e3,";
40 OUTPUT 717;"3E9,4E9,51,7e3,";
50 OUTPUT 717;"4E9,6E9,11,70e3"
60 OUTPUT 717;":SENS1:SEGM:LIST:CONT:DATA 1, 0, 0"
70 OUTPUT 717;":SENS1:SEGM:LIST:CONT:DATA?"
80 ENTER 717;H(*)