SCPI.SENSe(Ch).CORRection.CLEar

Type of object

Method (Write-only)

Syntax

SCPI.SENSe(Ch).CORRection.CLEar

Description

This command clears the error coefficient for calibration when the frequency offset feature is set to OFF, for the selected channel (Ch).

Example of use

SCPI.SENSe(1).CORRection.CLEar

Related objects

SCPI.SENSe(Ch).OFFSet.STATe

SCPI.SENSe(Ch).CORRection.OFFSet.CLEar

Equivalent key

Cal > Clear > OK

Equivalent SCPI command

Syntax

:SENSe{[1]-160}:CORRection:CLEar

Example of use

10 OUTPUT 717;":SENS1:CORR:CLE"