Property (Read-Write)
SCPI.SENSe(Ch).OFFSet.LOCal.CONTrol.STATe = Status
Status = SCPI.SENSe(Ch).OFFSet.LOCal.CONTrol.STATe
This command turns ON/OFF or return the status of the external signal source control mode, for the selected channel (Ch).
|
Parameter |
Status |
|
Description |
On/off of the external signal source |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following:
|
|
Preset value |
False or OFF |
Dim State As Boolean
SCPI.SENSe(1).OFFSet.LOCal.CONTrol.STATe = False
State = SCPI.SENSe(1).OFFSet.LOCal.CONTrol.STATe
Sweep Setup > Frequency Offset > External Source > Control
:SENSe{[1]-160}:OFFSet:LOCal:CONTrol[:STATe] {ON|OFF|1|0}
:SENSe{[1]-160}:OFFSet:LOCal:CONTrol[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":SENS1:OFFS:LOC:CONT ON"
20 OUTPUT 717;":SENS1:OFFS:LOC:CONT?"
30 ENTER 717;A