Property (Read-Write)
SCPI.SOURce(Ch).POWer.SPAN = Value
Value = SCPI.SOURce(Ch).POWer.SPAN
This command sets/gets the span value of the sweep range for the power sweep for the channels 1 to 36 (Ch).
|
Parameter |
Value |
|
Description |
Span value |
|
Data type |
Double precision floating point type (Double) |
|
Range |
Varies depending on the power range: 9 kHz to 5 GHz –55 to 10 dBm 5 to 6 GHz –55 to 9 dBm 6 to 7 GHz –55 to 8 dBm 7 to 8.5 GHz –55 to 7 dBm |
|
Preset value |
15 |
|
Unit |
dBm |
|
Resolution |
0.05 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Pspan As Double
SCPI.SOURce(1).POWer.SPAN = 10
Pspan = SCPI.SOURce(1).POWer.SPAN
SCPI.SOURce(Ch).POWer.ATTenuation.DATA
Span
:SOURce{[1]-160}:POWer:SPAN <numeric>
:SOURce{[1]-160}:POWer:SPAN?
{numeric}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:SPAN 10"
20 OUTPUT 717;":SOUR1:POW:SPAN?"
30 ENTER 717;A