Property (Read-Write)
SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.ENABle = Value
Value = SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.ENABle
This command sets/gets the value of the Questionable Bandwidth Limit Channel Extra Status Enable Register of the specified channel.
|
Parameter |
Value |
|
Description |
Value of the enable register |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 65535 |
|
Preset value |
Varies depending on the upper limit setting of the number of channels/traces. |
|
Note |
Bits 0 and 3 to 15 cannot be set to 1. |
For information on the variable (Ch), see Ch.
Dim Stat As Long
SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).ECHannel.ENABle = 6
Stat = SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).ECHannel.ENABle
SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ENABle
No equivalent key is available on the front panel.
:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:ECHannel:ENABle <numeric>
:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:ECHannel:ENABle?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:ECH:ENAB 6"
20 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:ECH:ENAB?"
30 ENTER 717;A