Property (Read-Write)
SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.NTRansition = Value
Value = SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.NTRansition
This command sets/gets the value of the negative transition filter of the "Questionable Bandwidth Limit Channel Extra Status Register" of the specified channel.
|
Parameter |
Value |
|
Description |
The value of the negative transition filter of the Questionable Bandwidth Limit Channel Extra Status Register |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 65535 |
|
Preset value |
0 |
|
Note |
Bits 0 and 3 to 15 cannot be set to 1. |
For information on the variable (Ch), see Ch.
Dim Stat As Long
SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).ECHannel.NTRansition = 6
Stat = SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).ECHannel.NTRansition
SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.EVENt
SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).ECHannel.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:ECHannel:NTRansition <numeric>
:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}:ECHannel:NTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:ECH:NTR 6"
20 OUTPUT 717;":STAT:QUES:BLIM:CHAN1:ECH:NTR?"
30 ENTER 717;A