Property (Read-Write)
SCPI.STATus.QUEStionable.BLIMit.ELIMit.NTRansition = Value
Value = SCPI.STATus.QUEStionable.BLIMit.ELIMit.NTRansition
This command sets/gets the value of the negative transition filter of the Questionable Bandwidth Limit Extra Status Register.
|
Parameter |
Value |
|
Description |
The value of the negative transition filter of the Questionable Bandwidth Limit Extra Status Register. |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 65535 |
|
Preset value |
0 |
|
Note |
Bits 0 and 3 to 15 cannot be set to 1. |
Dim Stat As Long
SCPI.STATus.QUEStionable.BLIMit.ELIMit.NTRansition = 6
Stat = SCPI.STATus.QUEStionable.BLIMit.ELIMit.NTRansition
SCPI.STATus.QUEStionable.BLIMit.ELIMit.EVENt
SCPI.STATus.QUEStionable.BLIMit.ELIMit.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:BLIMit:ELIMit:NTRansition <numeric>
:STATus:QUEStionable:BLIMit:ELIMit:NTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:BLIM:ELIM:NTR 6"
20 OUTPUT 717;":STAT:QUES:BLIM:ELIM:NTR?"
30 ENTER 717;A