Property (Read-Write)
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.PTRansition = Value
Value = SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.PTRansition
This command sets/gets the value of the positive transition filter of the Questionable Ripple Limit Channel Extra Status Register of the specified channel.
|
Parameter |
Value |
|
Description |
The value of the positive transition filter of the Questionable Ripple Limit Channel Extra Status Register. |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 65535 |
|
Preset value |
Varies depending on the upper limit setting of the number of channels/traces. |
|
Note |
Bits 0 and 3 to 15 cannot be set to 1. |
For information on the variable (Ch), see Ch.
Dim Stat As Long
SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).ECHannel.PTRansition = 6
Stat = SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).ECHannel.PTRansition
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.EVENt
SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.NTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:ECHannel:PTRansition <numeric>
:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:ECHannel:PTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:ECH:PTR 6"
20 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:ECH:PTR?"
30 ENTER 717;A