SCPI.SYSTem.BEEPer.COMPlete.IMMediate

Object type

Method (Write-only)

Syntax

SCPI.SYSTem.BEEPer.COMPlete.IMMediate

Description

This command generates a beep for the notification of the completion of an operation.

Examples

SCPI.SYSTem.BEEPer.COMPlete.IMMediate

Related objects

SCPI.SYSTem.BEEPer.COMPlete.STATe

SCPI.SYSTem.BEEPer.WARNing.IMMediate

Equivalent key

System > Misc Setup > Beeper > Test Beep Complete

Equivalent SCPI command

Syntax

:SYSTem:BEEPer:COMPlete:IMMediate

Example of use

10 OUTPUT 717;":SYST:BEEP:COMP:IMM"