SCPI.SYSTem.PRESet

Object type

Method (Write-only)

Syntax

SCPI.SYSTem.PRESet

Description

This command presets the setting state of the E5071C to the original factory setting (Default Conditions). This command is different from SCPI.IEEE4882.RSTas the continuous startup mode (see SCPI.INITiate(Ch).CONTinuous) of channel 1 is set to ON.

Examples

SCPI.SYSTem.PRESet

Related objects

SCPI.IEEE4882.RST

SCPI.SYSTem.UPReset

Equivalent key

Preset > OK

Equivalent SCPI command

Syntax

:SYSTem:PRESet

Example of use

10 OUTPUT 717;":SYST:PRES"