Property (Read-Write)
SCPI.TRIGger.SEQuence.AVERage = Status
Status = SCPI.TRIGger.SEQuence.AVERage
This command turns ON/OFF or gets the status of the averaging trigger function.
The sweep averaging feature must be set to ON when turning on the averaging trigger feature.
|
Parameter |
Status |
|
Description |
On/off status of the averaging trigger |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from either of the following.
|
|
Preset value |
False or OFF |
Dim Avetrig as Boolean
SCPI.TRIGger.SEQuence.AVERage = True
Avetrig = TRIGger.SEQuence.AVERage
Ave > Ave Trigger
:TRIGger[:SEQuence]:AVERage {ON|OFF|1|0}
:TRIGger[:SEQuence]:AVERage?
{1|0}<newline><^END>
10 OUTPUT 717;":TRIG:AVER ON"
20 OUTPUT 717;":TRIG:AVER?"
30 ENTER 717;A
For a complete sample program using VBA, please refer to Averaging Sample Program.