Property (Read-Write)
SCPI.TRIGger.SEQuence.SOURce = Param
Param = SCPI.TRIGger.SEQuence.SOURce
This command sets/gets the trigger source from the following 4 types:
Internal Trigger
Uses the internal trigger to generate continuous triggers automatically.
External Trigger
Generates a trigger when the trigger signal is inputted externally via the Ext Trig connector or the handler interface.
Manual Trigger
Generates a trigger when the key operation of Trigger > Trigger is executed from the front panel.
Bus Trigger
Generates a trigger when the SCPI.IEEE4882.TRG object is executed.
When you change the trigger source during sweep, the sweep is aborted.
|
Parameter |
Param |
|
Description |
Trigger source |
|
Data type |
Character string type (String) |
|
Range |
Select from either of the following:
|
|
Preset value |
"INTernal" |
Dim TrigSour As String
SCPI.TRIGger.SEQuence.SOURce = "bus"
TrigSour = SCPI.TRIGger.SEQuence.SOURce
Trigger > Trigger Source > Internal|External|Manual|Bus
:TRIGger[:SEQuence]:SOURce {INTernal|EXTernal|MANual|BUS}
:TRIGger[:SEQuence]:SOURce?
{BUS|EXT|INT|MAN}<newline><^END>
10 OUTPUT 717;":TRIG:SOUR BUS"
20 OUTPUT 717;":TRIG:SOUR?"
30 ENTER 717;A$