Analyzing impedance

By turning on the parameter conversion function, you can convert the measurement result of the S parameter to the following parameters.

To turn On/Off the parameter conversion function, use the following command:

:CALC{1-36}:CONV

To select the parameter to which you want to convert the measurement result, use the following command:

:CALC{1-36}:CONV:FUNC

Other topics about Analyzing Data