Statistical Analysis

The E5071C provides a mechanism that analyzes trace statistics. You can analyze the following statistics:

To retrieve the results of statistical analysis, use the following command:

:CALC{1-36}:MST:DATA?

Also, you can use the following command to control whether to display the results of statistical analysis on the LCD:

:CALC{1-36}:MST

Alternatively, you can use the analysis commands to analyze the trace statistics. When you use the analysis commands, you can analyze the trace data in a specific range as well as the trace data throughout the entire sweep range. For information on how to use the analysis commands, refer to Analysis Commands.

Other topics about Analyzing Data