You can obtain test results by issuing a result retrieval command or through the status register.
You can obtain the test results at each measurement point by retrieving the stimulus value at failed measurement points. To retrieve failed measurement points, use the following command:
|
Stimulus value |
:CALC{1-36}:LIM:REP? |
|
Number of measurement points |
:CALC{1-36}:LIM:REP:POIN? |
You cannot use the status register to obtain the test results at each measurement point.
You can retrieve the test result for each trace (i.e., the trace-wide result that combines the results for all measurement points in a particular trace) by issuing the following command:
:CALC{1-36}:LIM:FAIL?The condition register and event register under the questionable limit channel {1-16} status register provide 14 bits that correspond to traces 1 to 14 and contain the test results (0: Pass, 1: Fail) for the respective traces; for example, you can obtain the test result for trace 1 from bit 1 and that for trace 14 from bit 14. The condition register and event register under the questionable limit channel {1-16} extra status register provide two bits that correspond to traces 15 to 16 and contain the test results (0: Pass, 1: Fail) for the respective traces; for example, you can obtain the test result for trace 15 from bit 1 and that for trace 16 from bit 2.
Every bit of the condition register is set to 0 when a measurement cycle is started. Upon completion of measurement, those bits that correspond to failed traces are set to 1.
If the corresponding bit of the positive transition filter is set to 1 (preset value), each bit of the event register is set to 1 when the corresponding bit of the condition register changes from 0 to 1 (indicating that the corresponding trace failed the test).
To retrieve the registers, use the following commands:
|
Questionable limit channel {1-16} status register |
|
|
Condition register |
:STAT:QUES:LIM:CHAN{1-16}:COND? |
|
Event register |
:STAT:QUES:LIM:CHAN{1-16}? |
|
Questionable limit channel {1-16} extra status register |
|
|
Condition register |
:STAT:QUES:LIM:CHAN{1-16}:ECH:COND? |
|
Event register |
:STAT:QUES:LIM:CHAN{1-16}:ECH? |
Although up to 36 channel is available on E5071C, the registers for limit test and Ripple/Bandwidth limit tests are for up to 16 channel.
No command is available that allows you to directly retrieve the test result for each channel (i.e., the channel-wide result that combines the results for all traces in a particular channel).
The questionable limit status event register provides 14 bits that correspond to channels 1 to 14 and contain the test results (0: Pass, 1: Fail) for the respective channels; for example, you can obtain the test result for channel 1 from bit 1 and that for channel 14 from bit 14. The questionable limit extra status event register provides nine bits that correspond to channels 1 to 2 and contain the test results (0: Pass, 1: Fail) for the respective channels; for example, you can obtain the test result for channel 15 from bit 1 and that for channel 16 from bit 2.
Every bit of the condition register is set to 0 after the event registers are cleared by the *CLS. Upon completion of measurement, if the channel-wide test result that combines the results for all traces in a channel is "fail," the corresponding bit of the condition register is set to 1.
If the corresponding bit of the positive transition filter is set to 1 (preset value), every bit of the event register is set to 1 when the corresponding bit of the condition register changes from 0 to 1.
To retrieve the registers, use the following commands:
|
Questionable limit status register |
|
|
Condition register |
:STAT:QUES:LIM:COND? |
|
Event register |
:STAT:QUES:LIM? |
|
Questionable limit extra status register |
|
|
Condition register |
:STAT:QUES:LIM:ELIM:COND? |
|
Event register |
:STAT:QUES:LIM:ELIM? |

No command is available that allows you to directly retrieve the overall test results that combine the test results for all channels.
The condition register and event register under the questionable status event register each provides bit 10, from which you can obtain the overall test result (0: Pass, 1: Fail).
The condition register's bit 10 is set to 0 after the event registers are cleared by the *CLS. Upon completion of measurement, this bit is set to 1 if the overall test result that combines the results for all channels is "fail."
If the positive transition filter's bit 10 is set to 1 (preset value), the event register's bit 10 is set to 1 when the condition register's bit 10 changes from 0 to 1.
To retrieve the condition register and event register under the questionable status event register, use the following commands:
|
Condition register |
:STAT:QUES:COND? |
|
Event register |
:STAT:QUES? |