Other topics about Saving and Recalling
To create a directory (folder), use the following command:
To delete a file or a directory, use the following command:
To copy a file, use the following command:
File transfer from the external controller to the E5071C can be possible by reading data from a file on the controller and then writing them to the file on the E5071C.
:MMEM:TRAN
Also, file transfer from the E5071C to the external controller can be possible by reading data from a file on the E5071C using the commands as query and then writing them to the file on the controller.
To retrieve information for the storage that is built in the E5071C (usage, property of file located in a specified directory), use the following command;
See the Transferring Files.