You can save the settings for measurement conditions and screen display to a file along with other instrument settings, and these settings can later be loaded from the file.
Once you have saved the measurement condition and screen display settings to a file, you can later load them whenever necessary; therefore, you can quickly modify the settings loaded from a file to create new settings without having to issue many commands.
To save the current settings to a file, use the following command:
:MMEM:STOR
To load the settings from a file, use the following command:
:MMEM:LOAD