Command/Query
:CALCulate:ATRaces:TIME:STEP:AMPLitude <numeric>
:CALCulate:ATRaces:TIME:STEP:AMPLitude?
This command sets step amplitude value for the transform function.
|
Description |
Stimulus amplitude level |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
1m to 5 |
|
Preset Value |
200m |
|
Unit |
volt |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":CALC:ATR:TIME:STEP:AMPL 100e-3"
20 OUTPUT 717;":CALC:ATR:TIME:STEP:AMPL?"
30 ENTER 717;A
Setup > Stim. Ampl. (under Basic)