Command Only
:MMEMory:LOAD:EYE:BPATtern <string>
This command loads the specified user bit pattern file. The extension of file should be .txt. The bit pattern editing is not available through the command.
|
Description |
File name of user bit pattern (.txt) |
|
Data Type |
Character string type (String) |
|
Range |
- |
|
Preset Value |
- |
|
Unit |
- |
|
Resolution |
- |
10 OUTPUT 717;":MMEM:LOAD:EYE:BPAT ""D:\TDR\userbit.txt"""
20 OUTPUT 717;":CALC:EYE:INP:BPAT:TYPE USER"
:CALCulate:EYE:INPut:BPATtern:TYPE
Eye/Mask > User Pattern (Under Bit Pattern) > Load