Off
The following two commands are sent when Max or Min is selected:
:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:TYPE
:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:TRACking
Rise Time (10-90%), Rise Time (20-80%)
The following two commands are send when Rise Time is selected:
:CALCulate:TRACe{Tr}:TTIMe:THReshold
:CALCulate:TRACe{Tr}:TTIMe:STATe
Δ Time