Command/Query
:TRIGger:AVERage {ON|OFF|1|0}
:TRIGger:AVERage?
This command sets averaging trigger on/off. When averaging trigger is on, one trigger makes one averaging measurement. For example, if the averaging factor is set at 16, one trigger makes a measurement for 16 times.
|
Description |
Status of Averaging trigger |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
{1|0}<newline><^END>
10 OUTPUT 717;":TRIG:MODE HOLD"
20 OUTPUT 717;":SENS:AVER:COUN 16"
30 OUTPUT 717;":SENS:AVER:STAT ON"
40 OUTPUT 717;":TRIG:AVER ON"
50 OUTPUT 717;":TRIG:SING"
No equivalent GUI is available.