Command/Query
:TRIGger:MODE {HOLD|SINGle|RUN}
:TRIGger:MODE?
This command sets trigger mode.
|
Description |
Trigger mode |
|
Data Type |
Character string type (String) |
|
Range |
HOLD: Trigger is on hold until the conditions are meet, the trigger event starts. SINGle: Trigger event is run once. RUN: Trigger event is running continuous. |
|
Preset Value |
RUN |
|
Unit |
- |
|
Resolution |
- |
{HOLD|SINGle|RUN}<newline><^END>
10 OUTPUT 717;":TRIG:MODE HOLD"
20 OUTPUT 717;":TRIG:MODE?"
30 ENTER 717;A$
Stop Single or Run