Other topics about Application Programs
The apl_sys.vba shows a sample program (VBA program) that demonstrates how to measure a (3-terminal) duplexer. This VBA program consists of the following modules:
For the E5071C with 2-port S-parameter test set, a runtime error occurs because there are parameters that cannot be measured.
|
Object name |
Module type |
Description |
|
frmDupRes |
User form |
Displays the analysis result |
|
mdlDupMeas |
Standard module |
Performs duplexer measurement |
The program performs full 3-port calibration using the 85032F calibration kit, measures a (3-terminal) duplexer, and calculates and displays the limit test result, insertion loss, and band-pass ripple. The following figure shows the simple flow of the (3-terminal) duplexer measurement program:
Flow of duplexer measurement program

When you run this VBA program, reset is performed, the measurement conditions are set, and the message "Perform the full 3-port calibration" is displayed. To perform the full 3-port calibration, click Yes, otherwise click No.
To perform the calibration, follow the onscreen messages to connect each standard of the Keysight 85032F calibration kit to the specified port and then click OK to measure the calibration data. Click Cancel to return to the beginning of the calibration. You cannot skip the isolation calibration. When the calibration data measurement for all standards is complete, the message "All calibration data completion" is displayed, and the calibration coefficient is calculated.
When you cancel the calibration data measurement before completing the measurement of necessary calibration data, the settings conditions may not return to its original state.
Then, the limit line is set and the setting required for the limit test judgment is performed.
The message "Set the DUT between test cables." is displayed. Connect the DUT (duplexer) between the test cables and then click Yes. The limit line is set and a single sweep is executed. Then, for both trace 1 (Tx: S13) and trace 2 (Rx: S21), the Pass/Fail judgment of the limit test and the insertion loss and ripple analysis result within the pass band are displayed.
Click Exit on the user form displaying the analysis result. The message prompting for remeasurement is displayed. To perform remeasurement, click Yes, otherwise click No to terminate the program. The details of the program within the user form for displaying the analysis result (object name: frmDupRes) are not described here.
Display of the execution result of the program of "apl_sys.vba"

The duplexer measurement program (object name: mdlDupMeas) is described in detail below. Line numbers are added for description purpose only and do not appear in the actual program source code.
Stores the calibration kit number (4: 85032F) into the CalKit variable.
Turns off display update. Turning off display update shortens drawing time and object processing time.
Returns the E5071C to the preset state.
For channel 1, these lines turn the continuous trigger startup mode to On and sets the trigger source to the bus trigger.
Calls the Setup_Parameter procedure (lines 910 to 1140). For information on the Setup_Parameter procedure, see the description later.
Calls the Setup_Segment procedure (lines 1160 to 1530). For information on the Setup_Segment procedure, see the description later.
Stores the calibration kit number for channel 1 into the CalKit variable.
Stores 1, 2, and 3 into the Port variable that indicates the ports used for the full 3-port calibration.
Calls the Calib_Solt procedure.
Calls the Setup_Limitline procedure (lines 2420 to 3180). For information on the Setup_Limitline procedure, see the description later.
Calls the Setup_Register procedure (lines 3200 to 3260). For information on the Setup_Register procedure, see the description later.
Displays the message that prompts for connecting a DUT (Device Under Test) and waits for the OK button to be clicked after the connection.
Clears the questionable limit status event register and questionable limit channel 1 status event register.
Generate a trigger to start a single sweep and wait until the measurement finishes (1 is read out with the SCPI.IEEE4882.OPC object).
For traces 1 and 2, these lines executes the auto scale to set the optimum scale.
Read out the value of the questionable limit status event register and store the AND of the read-out value and 2 (the value in which only bit 1 is 1) into the Test_Ch1 variable.
Read out the value of the questionable limit channel 1 status event register and store the AND of the read-out value and 2 (the value in which only bit 1 is 1) into the Test_Tr1 variable and the AND of the read-out value and 4 (the value in which only bit 2 is 1) into the Test_Tr2 variable.
Specify trace 1 as the active trace and set the analysis range (start point: 1.85 GHz and stop point: 1.91 GHz). Then these lines sets the polarity of the peak search (both the positive peak and the negative peak) and the lower limit of the peak excursion value (0).
Search for the minimum value within the analysis range and store the analysis result into the IlossTx variables.
Uses the ripple analysis function to store the maximum value of the response differences between the positive peaks and the negative peaks within the analysis range into the RipTx variables.
Specify trace 2 as the active trace and set the analysis range (start point: 1.93 GHz and stop point: 1.99 GHz). Then these lines set the polarity of the peak search (both the positive peak and the negative peak) and the lower limit of the peak excursion value (0).
Search for the minimum value within the analysis range and store the analysis result into the IlossRx variables.
Uses the ripple analysis function to store the maximum value of the response differences between the positive peaks and the negative peaks within the analysis range into the RipRx variables.
Calls the Display_Update procedure (lines 3280 to 3620). For information on the Display_Update procedure, see the description later.
Displays the user form (object name: frmDupRes) on the screen to display the analysis result.
Display the message asking whether you want to perform measurement again. Click the Yes button to return to the DUT connection section. Click the No button to terminate the program.
Store the channel layout ("D1": 1-channel display), graph layout ("D1_2": upper/lower 2 part split display), measurement parameter of trace 1 (S13), measurement parameter of trace 2 (S21), data format of trace 1 (MLOG), and data format of trace 2 (MLOG) into the ChDisp, TracDisp, Par(0), Par(1), Fmt(0), and Fmt(1) variables, respectively.
Set the number of traces for channel 1 to 2, the channel layout to the ChDisp variable, and the graph layout for channel 1 to the TracDisp variable.
Set the measurement parameter for trace 1 to the Par(0) variable, the data format for trace 1 to the Fmt(0) variable, the measurement parameter for trace 2 to the Par(1) variable, and the data format for trace 2 to the Fmt(1) variable.
Store the conditions for channel 1's segment table setting into the SegmData(0) to SegmData(6) variables. The settings are as follows. Stimulus setting mode: start/stop value. IF bandwidth setting for each segment: off. Power setting for each segment: off. Sweep delay time setting for each segment: off. Sweep time setting for each segment: off. Number of segments: 5.
Store the sweep start value, the sweep stop value, and the number of measurement points for channel 1's segments 1 through 5 into the SegmData(7) to SegmData(21) variables, respectively.
Sets channel 1's segment table to the SegmData variable.
Sets channel 1's sweep type to "segment".
Sets the channel 1 graph's horizontal axis display method to the order base (the axis on which the measurement point numbers are placed evenly in the order of measurement).
See Lines 1200 to 2130 of Calib_Solt.
Stores the number of lines (5) in trace 1 limit table into the LimDataS13(0) variable.
Store the settings in trace 1 limit table into the LimDataS13(1) to LimDataS13(25) variables.
Stores the number of lines (4) in trace 2 limit table into the LimDataS21(0) variable.
Store the settings in trace 2 limit table into the LimDataS21(1) to LimDataS21(20) variables.
Specify trace 1 as the active trace, store trace 1's limit line into the LimDataS13 variable, and display it. Then, these lines turn on the limit test function for trace 1.
Specify trace 2 as the active trace, store trace 2's limit line into the LimDataS21 variable, and display it. Then, these lines turn on the limit test function for trace 2.
Set the instrument so that the questionable limit channel status event register's bits 1 and 2 are set to 1 only when the questionable limit channel status register's bits 1 and 2 are changed from 0 to 1 (positive transition).
Enables the questionable limit channel status event register's bits 1 and 2.
Updates the display on the LCD screen once.
When trace 1's limit test result is Fail (Test_Tr1 = 2), these lines display Tx(S13) "Limit test result: Fail" on the user form (object name: frmDupRes) against a red background. On the other hand, when trace 1's limit test result is Pass (Test_Tr1 ¼ 2), they display Tx(S13) "Limit test result: Pass" on the user form (object name: frmDupRes) against a blue background.
When trace 2's limit test result is Fail (Test_Tr2 = 4), these lines display Rx(S21) "Limit test result: Fail" on the user form (object name: frmDupRes) against a red background. On the other hand, when trace 1's limit test result is Pass (Test_Tr2 ≠ 4), they display Rx(S21) "Limit test result: Pass" on the user form (object name: frmDupRes) against a blue background.
When channel 1's limit test result is Fail (Test_Ch1 = 2), these lines display "Overall limit test result: Fail" on the user form (object name: frmDupRes) against a red background. On the other hand, when channel 1's limit test result is Pass (Test_Ch1 ≠ 2), they display "Overall limit test result: Pass" on the user form (object name: frmDupRes) against a blue background.
Display the analysis results for traces 1 and 2 (insertion loss and band-pass ripple) as Tx(S13) and Rx(S21), respectively, on the user form (object name: frmDupRes).
Duplexer measurement (object name: mdlDupMeas)
10| Sub Main()
20|
30| Dim CalKit As Long, Dmy As Long, Rgst As Long, I As Long, Buff As Long
40| Dim Test_Ch1 As Integer, Test_Tr1 As Integer, Test_Tr2 As Integer
50| Dim IlossTx As Variant, IlossRx As Variant
60| Dim RipTx As Double, RipRx As Double
70| Dim Port As Variant
80|
90| CalKit = 4 'Calibration kit :85032F
100|
110| SCPI.DISPlay.ENABle = False
120|
130| '''Presetting the E5071C
140| SCPI.SYSTem.PRESet
150|
160| '''Setting measurement conditions
170| SCPI.INITiate(1).CONTinuous = True
180| SCPI.TRIGger.SEQuence.Source = "BUS"
190|
200| Setup_Parameter
210|
220| Setup_Segment
230|
240| '''Full 3-port calibration
250| SCPI.SENSe(1).CORRection.COLLect.CKIT.Select = CalKit
260| Port = Array(1, 2, 3)
270|
280| Calib_Solt 1, 3, Port
290|
300| '''Setting analysis conditions
310| Setup_Limitline
320|
330| Setup_Register
340|
350| Meas_Start:
360|
370| '''Connecting DUT
380| MsgBox "Connect DUT between test cables."
390|
400| '''Performing single sweep
410| SCPI.IEEE4882.CLS
420| SCPI.TRIGger.SEQuence.SINGle
430| Dmy = SCPI.IEEE4882.OPC
440|
450| SCPI.DISPlay.WINDow(1).TRACe(1).Y.SCALe.AUTO
460| SCPI.DISPlay.WINDow(1).TRACe(2).Y.SCALe.AUTO
470|
480| '''Judging limit test
490| Rgst = SCPI.STATus.QUEStionable.LIMit.EVENt
500| Test_Ch1 = CInt(Rgst And 2)
510| Rgst = SCPI.STATus.QUEStionable.LIMit.CHANnel(1).EVENt
520| Test_Tr1 = CInt(Rgst And 2)
530| Test_Tr2 = CInt(Rgst And 4)
540|
550| '''Analyzing insertion loss/bandpass ripple
560| SCPI.CALCulate(1).PARameter(1).Select
570| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STARt = 1850000000#
580| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STOP = 1910000000#
590| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STATe = True
600| SCPI.CALCulate(1).SELected.FUNCtion.PPOLarity = "both"
610| SCPI.CALCulate(1).SELected.FUNCtion.PEXCursion = 0
620| SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "MIN"
630| SCPI.CALCulate(1).SELected.FUNCtion.EXECute
640| IlossTx = SCPI.CALCulate(1).SELected.FUNCtion.DATA
650| RipTx = MaxPeakToPeak(1)
660|
670| SCPI.CALCulate(1).PARameter(2).Select
680| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STARt = 1930000000#
690| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STOP = 1990000000#
700| SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STATe = True
710| SCPI.CALCulate(1).SELected.FUNCtion.PPOLarity = "both"
720| SCPI.CALCulate(1).SELected.FUNCtion.PEXCursion = 0
730| SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "MIN"
740| SCPI.CALCulate(1).SELected.FUNCtion.EXECute
750| IlossRx = SCPI.CALCulate(1).SELected.FUNCtion.DATA
760| RipRx = MaxPeakToPeak(1)
770|
780| '''Displaying the results
790| Display_Update Test_Tr1, Test_Tr2, Test_Ch1, IlossTx, IlossRx, RipTx, RipRx
800|
810| frmDupRes.Show
820|
830| Buff = MsgBox("Do you make another measurement?", vbYesNo, "Duplexer Measurement")
840|
850| If Buff = vbYes Then
860| GoTo Meas_Start
870| End If
880|
890| End Sub
900|
910| Private Sub Setup_Parameter()
920|
930| Dim I As Long
940| Dim ChDisp As String, TracDisp As String
950| Dim Par(1) As String, Fmt(1) As String
960|
970| ChDisp = "D1"
980| TracDisp = "D1_2"
990| Par(0) = "S13"
1000| Par(1) = "S21"
1010| Fmt(0) = "MLOG"
1020| Fmt(1) = "MLOG"
1030|
1040| SCPI.CALCulate(1).PARameter.Count = 2
1050| SCPI.DISPlay.Split = ChDisp
1060| SCPI.DISPlay.WINDow(1).Split = TracDisp
1070|
1080| For I = 1 To 2
1090| SCPI.CALCulate(1).PARameter(I).DEFine = Par(I - 1)
1100| SCPI.CALCulate(1).PARameter(I).Select
1110| SCPI.CALCulate(1).SELected.Format = Fmt(I - 1)
1120| Next I
1130|
1140| End Sub
1150|
1160| Private Sub Setup_Segment()
1170|
1180| Dim SegmData(21) As Variant
1190|
1200| SegmData(0) = 5 'Anytime 5 is set at seg ment settings
1210| SegmData(1) = 0 'Allows stimulus range to be set using Start/Stop frequency
1220| SegmData(2) = 0 'Not allows IF bandwidth to be set
1230| SegmData(3) = 0 'Not allows power to be set
1240| SegmData(4) = 0 'Not allows delay time to be set
1250| SegmData(5) = 0 'Not allows sweep time to be set
1260| SegmData(6) = 5 'Number of segments
1270|
1280| '''Segment 1
1290| SegmData(7) = 1730000000# 'Start frequency
1300| SegmData(8) = 1830000000# 'Stop frequency
1310| SegmData(9) = 50 'Number of points
1320| '''Segment 2
1330| SegmData(10) = 1830000000# 'Start frequency
1340| SegmData(11) = 2030000000# 'Stop frequency
1350| SegmData(12) = 400 'Number of points
1360| '''Segment 3
1370| SegmData(13) = 2030000000# 'Start frequency
1380| SegmData(14) = 2130000000# 'Stop frequency
1390| SegmData(15) = 50 'Number of points
1400| '''Segment 4
1410| SegmData(16) = 3650000000# 'Start frequency
1420| SegmData(17) = 4030000000# 'Stop frequency
1430| SegmData(18) = 38 'Number of points
1440| '''Segment 5
1450| SegmData(19) = 5500000000# 'Start frequency
1460| SegmData(20) = 6020000000# 'Stop frequency
1470| SegmData(21) = 52 'Number of points
1480|
1490| SCPI.SENSe(1).SEGMent.DATA = SegmData
1500| SCPI.SENSe(1).SWEep.TYPE = "SEGM"
1510| SCPI.DISPlay.WINDow(1).X.SPACing = "OBAS"
1520|
1530| End Sub
1540|
1550| Private Sub Calib_Solt(Chan As Long, SoltType As Long, Port A s Variant)
1560|
1570| Dim Dmy As Long, I As Long, J As Long, Buff As Long
1580|
1590| Cal_Start:
1600|
1610| Buff = MsgBox("Perform the full " & SoltType & "-port calib ration.", vbOKCancel, "Full" & SoltType & "-port calibration")
1620| If Buff = vbCancel Then
1630| GoTo Cal_Skip
1640| End If
1650|
1660| Select Case SoltType
1670| Case 1
1680| SCPI.SENSe(Chan).CORRection.COLLect.METHod.SOLT1 = Port(0)
1690| Case 2
1700| SCPI.SENSe(Chan).CORRection.COLLect.METHod.SOLT2 = Port
1710| Case 3
1720| SCPI.SENSe(Chan).CORRection.COLLect.METHod.SOLT3 = Port
1730| Case 4
1740| SCPI.SENSe(Chan).CORRection.COLLect.METHod.SOLT4 = Port
1750| End Select
1760|
1770| For I = 1 To SoltType
1780|
1790| Buff = MsgBox("Connect the Open standard to Port " & CS tr(Port(I - 1)) & ".", vbOKCancel, "Full" & SoltType & "-port calibr ation")
1800| If Buff = vbOK Then
1810| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.OPEN = Port(I - 1)
1820| Dmy = SCPI.IEEE4882.OPC
1830| Else
1840| GoTo Cal_Start
1850| End If
1860|
1870| Buff = MsgBox("Connect the Short standard to Port " & C Str(Port(I - 1)) & ".", vbOKCancel, "Full" & SoltType & "-port calib ration")
1880| If Buff = vbOK Then
1890| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.Short = Port(I - 1)
1900| Dmy = SCPI.IEEE4882.OPC
1910| Else
1920| GoTo Cal_Start
1930| End If
1940|
1950| Buff = MsgBox("Connect the Load standard to Port " & CS tr(Port(I - 1)) & ".", vbOKCancel, "Full" & SoltType & "-port calibr ation")
1960| If Buff = vbOK Then
1970| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.Load = Port(I - 1)
1980| Dmy = SCPI.IEEE4882.OPC
1990| Else
2000| GoTo Cal_Start
2010| End If
2020| Next I
2030|
2040| For I = 1 To SoltType - 1
2050| For J = I + 1 To SoltType
2060| Buff = MsgBox("Connect the Thru standard between Por t " & CStr(Port(I - 1)) & " and Port " & CStr(Port(J - 1)) & ".", vb OKCancel, "Full" & SoltType & "-port calibration")
2070| If Buff = vbOK Then
2080| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.THRU = Array(Port(I - 1), Port(J - 1))
2090| Dmy = SCPI.IEEE4882.OPC
2100| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.THRU = Array(Port(J - 1), Port(I - 1))
2110| Dmy = SCPI.IEEE4882.OPC
2120| Else
2130| GoTo Cal_Start
2140| End If
2150| Next J
2160| Next I
2170|
2180| If SoltType <> 1 Then
2190| Buff = MsgBox("Do you measure the Isolation (Optional)? ", vbYesNo, "Full" & SoltType & "-port calibration")
2200| If Buff = vbYes Then
2210| For I = 1 To SoltType - 1
2220| For J = I + 1 To SoltType
2230| Buff = MsgBox("Connect the Load standard to Port " & Port(I - 1) & " and Port " & Port(J - 1) & ".", vbOKCancel, "Full" & SoltType & "-port calibration")
2240| If Buff = vbOK Then
2250| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.ISOLation = Array(Port( I - 1), Port(J - 1))
2260| Dmy = SCPI.IEEE4882.OPC
2270| SCPI.SENSe(Chan).CORRection.COLLect.ACQuire.ISOLation = Array(Port( J - 1), Port(I - 1))
2280| Dmy = SCPI.IEEE4882.OPC
2290| Else
2300| GoTo Cal_Start
2310| End If
2320| Next J
2330| Next I
2340| End If
2350| End If
2360|
2370| SCPI.SENSe(1).CORRection.COLLect.SAVE
2380| MsgBox "All calibration data completion."
2390|
2400| Cal_Skip:
2410|
2420| End Sub
2430|
2440| Private Sub Setup_Limitline()
2450|
2460| Dim LimDataS13(25) As Variant, LimDataS21(20) As Variant
2470|
2480| '''Limit line for S13
2490| LimDataS13(0) = 5 'Number of segment
2500| '''Limit_line 1
2510| LimDataS13(1) = 1 'Maximum
2520| LimDataS13(2) = 1730000000# 'Beginning of stimulus
2530| LimDataS13(3) = 1930000000# 'End of stimulus
2540| LimDataS13(4) = 0 'Beginning of response
2550| LimDataS13(5) = 0 'End of response
2560| '''Limit_line 2
2570| LimDataS13(6) = 2 'Minimum
2580| LimDataS13(7) = 1850000000# 'Beginning of stimulus
2590| LimDataS13(8) = 1910000000# 'End of stimulus
2600| LimDataS13(9) = -8 'Beginning of response
2610| LimDataS13(10) = -8 'End of response
2620| '''Limit_line 3
2630| LimDataS13(11) = 1 'Maximum
2640| LimDataS13(12) = 1930000000# 'Beginning of stimulus
2650| LimDataS13(13) = 1990000000# 'End of stimulus
2660| LimDataS13(14) = -35 'Beginning of response
2670| LimDataS13(15) = -35 'End of response
2680| '''Limit_line 4
2690| LimDataS13(16) = 1 'Maximum
2700| LimDataS13(17) = 1990000000# 'Beginning of stimulus
2710| LimDataS13(18) = 2130000000# 'End of stimulus
2720| LimDataS13(19) = -40 'Beginning of response
2730| LimDataS13(20) = -40 'End of response
2740| '''Limit_line 5
2750| LimDataS13(21) = 1 'Maximum
2760| LimDataS13(22) = 2130000000# 'Beginning of stimulus
2770| LimDataS13(23) = 6020000000# 'End of stimulus
2780| LimDataS13(24) = -20 'Beginning of response
2790| LimDataS13(25) = -20 'End of response
2800|
2810| '''Limit line for S21
2820| LimDataS21(0) = 4 'Number of segment
2830| '''Limit_line 1
2840| LimDataS21(1) = 1 'Maximum
2850| LimDataS21(2) = 1730000000# 'Beginning of stimulus
2860| LimDataS21(3) = 1850000000# 'End of stimulus
2870| LimDataS21(4) = -40 'Beginning of response
2880| LimDataS21(5) = -40 'End of response
2890| '''Limit_line 2
2900| LimDataS21(6) = 1 'Maximum
2910| LimDataS21(7) = 1850000000# 'Beginning of stimulus
2920| LimDataS21(8) = 1910000000# 'End of stimulus
2930| LimDataS21(9) = -40 'Beginning of response
2940| LimDataS21(10) = -40 'End of response
2950| '''Limit_line 3
2960| LimDataS21(11) = 1 'Maximum
2970| LimDataS21(12) = 1910000000# 'Beginning of stimulus
2980| LimDataS21(13) = 6020000000# 'End of stimulus
2990| LimDataS21(14) = 0 'Beginning of response
3000| LimDataS21(15) = 0 'End of response
3010| '''Limit_line 4
3020| LimDataS21(16) = 2 'Minimum
3030| LimDataS21(17) = 1930000000# 'Beginning of stimulus
3040| LimDataS21(18) = 1990000000# 'End of stimulus
3050| LimDataS21(19) = -10 'Beginning of response
3060| LimDataS21(20) = -10 'End of response
3070|
3080| SCPI.CALCulate(1).PARameter(1).Select
3090| SCPI.CALCulate(1).SELected.LIMit.DATA = LimDataS13
3100| SCPI.CALCulate(1).SELected.LIMit.DISPlay.STATe = True
3110| SCPI.CALCulate(1).SELected.LIMit.STATe = True
3120|
3130| SCPI.CALCulate(1).PARameter(2).Select
3140| SCPI.CALCulate(1).SELected.LIMit.DATA = LimDataS21
3150| SCPI.CALCulate(1).SELected.LIMit.DISPlay.STATe = True
3160| SCPI.CALCulate(1).SELected.LIMit.STATe = True
3170|
3180| End Sub
3190|
3200| Private Sub Setup_Register()
3210|
3220| SCPI.STATus.QUEStionable.LIMit.CHANnel(1).PTRansition = 6
3230| SCPI.STATus.QUEStionable.LIMit.CHANnel(1).NTRansition = 0
3240| SCPI.STATus.QUEStionable.LIMit.CHANnel(1).ENABle = 6
3250|
3260| End Sub
3270|
3280| Sub Display_Update(Test_Tr1 As Integer, Test_Tr2 As Integer, Test_Ch1 As Integer, IlossTx As Variant, IlossRx As Variant, RipTx As Variant, RipRx As Variant)
3290|
3300| SCPI.DISPlay.UPDate.IMMediate
3310|
3320| If Test_Tr1 = 2 Then
3330| frmDupRes.lblJudgeS13.BackColor = RGB(255, 0, 0)
3340| frmDupRes.lblJudgeS13.Caption = "Fail"
3350| Else
3360| frmDupRes.lblJudgeS13.BackColor = RGB(0, 0, 255)
3370| frmDupRes.lblJudgeS13.Caption = "Pass"
3380| End If
3390|
3400| If Test_Tr2 = 4 Then
3410| frmDupRes.lblJudgeS21.BackColor = RGB(255, 0, 0)
3420| frmDupRes.lblJudgeS21.Caption = "Fail"
3430| Else
3440| frmDupRes.lblJudgeS21.BackColor = RGB(0, 0, 255)
3450| frmDupRes.lblJudgeS21.Caption = "Pass"
3460| End If
3470|
3480| If Test_Ch1 = 2 Then
3490| frmDupRes.lblResult.BackColor = RGB(255, 0, 0)
3500| frmDupRes.lblResult.Caption = "Fail"
3510| Else
3520| frmDupRes.lblResult.BackColor = RGB(0, 0, 255)
3530| frmDupRes.lblResult.Caption = "Pass"
3540| End If
3550|
3560| frmDupRes.txtIlossS13.Text = Format(IlossTx(0), "0.#### ")
3570| frmDupRes.txtIlossS21.Text = Format(IlossRx(0), "0.#### ")
3580|
3590| frmDupRes.txtRipS13.Text = Format(RipTx, "0.####")
3600| frmDupRes.txtRipS21.Text = Format(RipRx, "0.####")
3610|
3620| End Sub